跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can you please describe the function to detect stack-over in the ICE?

Latest Updated:12/01/2011

Question:

Please describe the function to detect stack-over in the ICE.

Answer:

Stack-over detection is enabled by setting "stack" for the memory attribute in the configuration dialog box.

(Reference)
ID78K4 User's Manual
Debug window
Configuration dialog box


Moreover, to test the size actually consumed as the stack, fill the memory capacity in the vicinity of the stack with a special value prior to program execution, and following program execution, count the bytes that have been overwritten.
Determining the number of overwritten bits on the memory display is easy when using 0x11 as the special value.

Suitable Products
78K Family