跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I use HEW on Windows XP SP(Service Pack)2 ?

Latest Updated:09/10/2007

Question:

Can I use HEW on Windows XP SP(Service Pack)2 ?

Answer:

As to the support status for Windows XP Service Pack2, please refer to the following URL.

http://tool-support.renesas.com/eng/toolnews/n050301/tn18.htm

Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family