跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can ES MCU be shipped to confirm the contents of the programmed ROM?

Latest Updated:09/15/2006

Question:

[QzROM, R8C/Tiny] Can the ES MCU be shipped to confirm the contents of the programmed ROM?

Answer:

No, as a rule we do not ship the ES MCU.
So, confirm the ROM data file enough when submitting it, please.  Also, confirm the function of whole system with the first shipped MCU of mass production. If problem is found, you should contact your Renesas sales office as soon as possible. We judge as no problem, if you do not contact us for two weeks after the first shipment of mass production.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering