跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Are there restrictions on hexadecimal data file names?

Latest Updated:09/15/2006

Question:

Are there restrictions on hexadecimal data file names?

Answer:

With MM, file names which conform to the OS being used can be processed.

However, mask file names are written in 8 or 3 characters long, therefore it is necessary to rename any file which does not fit this condition.

MM adds the .MSK extension to the program file name and to the hexadecimal data file name specified with the PROG: identifier.

Therefore, if the program file name and the hexadecimal data file name specified with the PROG: identifier is 8 or 3 characters long, the mask file will have to be renamed.

Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering