跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Are the H8/300L series Flash devices in circuit programmable ?

Latest Updated:03/18/2009

Question:

Are the H8/300L series Flash devices in circuit programmable ?

Answer:

All Renesas flash micro-controllers can be programmed in circuit. Each device comes with a built in boot loader which allows the device to be programmed automatically from a host computer via the on-chip serial port. Full details of this can be found in the users manuals of each device.
Suitable Products
H8 Family
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power
  • 这篇文章对您有帮助吗?