跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

About Code Generator Plug-in setting when MCU is changed in CS+ or e² studio

Last Updated:08/02/2017

Question:

Are the Code Generator Plug-in settings deleted when an MCU is changed in CS+ or e² studio?

Answer:

When only the ROM/RAM size of an MCU is changed, the Code Generator Plug-in settings are inherited.
When the type or the number of pins of an MCU is changed, the Code Generator Plug-in settings are initialized without being inherited because the peripheral function or pin arrangement changes.

3000133-cs.PNG

For CS+:

For e² studio:

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator