跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

"Do I have to input MCU type data at a certain address with ASCII code? "

Latest Updated:09/15/2006

Question:

When I send a mask ROM order on a floppy disk, do I have to input the MCU type data at a certain address with ASCII code?

Answer:

No. When a mask ROM order is received in floppy disk form, the MCU type name is input during the mask data generation.
Therefore, you don't need to input the MCU type name.
In fact, if you do so, an error might occur in the ROM Mask generation process.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 这篇文章对您有帮助吗?