跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Tasks/interrupts do not work as expected while using the RI600V4

Last Updated:05/31/2017

Question:

Although using the real-time OS RI600V4, no interrupt occurs and tasks do not work as expected after the first interrupt handler is executed.

Answer:

Please make sure that the following header files are included in the source of the interrupt handler.
kernel.h
kernel_id.h

If using the source of a project without an OS, note the following:

The interrupt handler and the exception handler must be registered using a CF file.
Note: The source for the interrupt vector table is not needed.

If "#pragma interrupt <interrupt-handler-function name>...” is written in the line just before the interrupt handler function, delete or comment out the line.
Note: In the RI600V4, "#pragma interrupt <interrupt-handler-function name>..." is output in kernel_id.h that is generated by the configurator.

Do not declare the interrupt handler function as static.
Note: In the RI600V4, the function is referenced from the interrupt vector table that is generated by the configurator.

Suitable Products

RI600V4
RI600PX
  • 这篇文章对您有帮助吗?