跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Meaning of MCU Product Types under ITRON Agreement

Last Updated:02/21/2018

Question:

It is stated that, under the ITRON agreement, I need to make a contract for each product type of MCUs to be used. How are product types of MCUs differentiated in this case?

Answer:

The ITRON license agreement is limited to one device and one use (set), and product types are basically differentiated by device.

Suitable Products

RI600V4
RI600PX
RI78V4 V2
RI850V4 V2
RX Family
RL78 Family
RH850 Family