跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the status after the target board has been reset?

Latest Updated:07/31/2008

Question:

What is the operating status after the target board has been reset?

Answer:

M16C Family (M32C, M16C/60 or R8C/Tiny Series) or the 740 Family:
We recommend you do not reset the target board during a break, as the E8a emulator may no longer operate properly.
Always use the High-performance Embedded Workshop command to execute a reset.
If the target board is reset during a RUN, the user program will break at that point.

H8 Family:
H8 Family MCU specifications do not allow the MCU to accept a reset during a break. Therefore, this will not affect the operations of the E8a emulator.
If the target board is reset during a RUN, the user program is reset.
Suitable Products
E8a