跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What are the differences of HS0005KCU01H and HS0005KCU02H?

Latest Updated:03/14/2011

Question:

What are the functional differences of E10A-USB emulators HS0005KCU01H (no AUD function) and HS0005KCU02H (with AUD function)?

Answer:

The HS0005KCU02H (with AUD function) offers a more enhanced trace function compared to that of HS0005KCU01H (no AUD function). (Enhanced functions vary according to MCU)

For details on the AUD Trace, click here for a list of major debugging functions.
Suitable Products
E10A-USB