跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Unable to open memory or extended monitor window when using Emulator_HEW

Last Updated:10/11/2017

Question:

I am using one of the Suitable Products listed below with High-performance Embedded Workshop V.3, but I am unable to open the memory window or the extended monitor window. When I go to the menu bar and open [View -> CPU -> Memory] or [View -> CPU -> Extended Monitor] , the memory display is dimmed and unavailable.
What is the cause and solution for this?

Answer:

Most likely the memory window or extended monitor window is in the hidden state while more than the allowable number of windows are open at the same time.

As shown in the figure below, you can display a list of all currently open windows by floating any menu bar (excluding the title bar) and right-clicking inside the box outlined in red. The items that are marked with a check are visible windows. Add a check next to the window name(memory or extended monitor) that problem occurs to put the memory window( or extended memory window) in the visible state. Finally, close the memory window( or Extended Monitor Window) that the problem had occurred while it is in the visible state.

Note: The Extended Monitor Window is supported on some products.

emulator_107362.JPG

Suitable Products

E10A-USB
E8a
E10T-USB
E10A
E8
E7
E100
R0E0200F0EMU00
R0E0200F1EMU00
R0E0200F2EMU00
E6000H
E6000