跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

M16C family MCU: Contents of banks 0 to 6 aren't shown in Memory window

Latest Updated:06/20/2013

Question:

When using the M16C family MCU in the memory space expansion function 4 MB mode, the contents of banks 0 to 6 are not displayed in the Memory window or Watch window when performing debugging with the E100 emulator or E8a emulator.

Answer:

To access the memory space expansion area in the download, the editor window (MIX display or disassembled display mode), the memory window or the watch window while operating in the memory space expansion 4 MB mode, be aware that only bank 7 can be accessed. In this case, the data bank offset depends on the offset bits of the data bank register.

When using the memory space expansion function 4 MB mode, execute the command for the memory space expansion function 4 MB mode to access each bank. For more information about the memory space expansion function 4 MB mode, please refer to each emulator's help page.

Suitable Products
E8a
E100