跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

I cannot get the command to execute HEW

Last Updated:09/27/2017

Question:

After entering a command in the command line window in the High-performance Embedded Workshop, I can't get the command to execute.
(Example: I added the execute command (Go) but I can't execute the program.)

Answer:

Check to see if the "open bracket indicator" is blinking as shown below.

emulator_107033_en_GL_1.jpg

Try adding "]" to the command line window to terminate the blinking "open bracket indicator".

The "open bracket indicator" blinks when "[" is input to the command line window. In this case, the commands that are input while the indicator is blinking are held until the indicator goes off, and then executed.

Suitable Products

E8
E8a
E200F
E6000
E6000H
E10A-USB
E10T-USB
E100
E30A
PC4701L
PC4701M
PC4701U
PC7501
  • 这篇文章对您有帮助吗?