跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to properly download program in E10A USB Writing Flash memory mode?

Latest Updated:03/12/2008

Question:

When downloading a program in the E10A-USB Writing Flash memory mode, I get the following warning:
"The program size exceeds range of flash memory."

What is the cause of and solution for this problem?

Answer:

This message indicates the program was downloaded to the address other than in the internal ROM area on the MCU.

Refer to the map file to see if data exist in an address other than the on-chip ROM area, and modify your program so that the data is assigned to the internal ROM area.

Suitable Products
E10A-USB