跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to change the LCD RAM in RAM addresses 840h to 863h?

Latest Updated:08/08/2008

Question:

I can't change the LCD RAM in RAM addresses 840h to 863h when I debug a 38D5 Group MCU using E8a emulator software Version 1.00 Release 00.

Answer:

When using E8a emulator software Version 1.00 Release 00A or earlier, the RAM area used by the emulator and the LCD RAM area overlap. As a workaround, use E8a emulator software Version 1.01 Release 00 or later and set the RAM area for the emulator to an address other than that of the LCD RAM area. Click here to download the latest version of E8a emulator software.
Suitable Products
E8a