跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Error Message: starting E1/E20 emulator debugger in flash writer mode

Latest Updated:02/01/2012

Question:

When I start up the E1/E20 emulator debugger in the flash writer mode, the following error message is generated. How can I resolve this problem?

Error: Failed in the acquisition of the memory.

Answer:

This error message is displayed when the workspace you have started up has a window open that does not support use of the flash writer mode (image window or waveform window).
If this error message is generated, download the program after closing the windows described above.
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]