跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does device group of E10A-USB need to be specified at time of purchase?

Latest Updated:06/10/2011

Question:

I realize that the purchase of the E10A-USB includes one device group license, but does that device group need to be specified at the time of purchase?

Answer:

No, you do not need to specify the device group when you purchase the E10A-USB. The device group is selected when you install the E10A-USB software.

For details refer to the following:

Suitable Products
E10A-USB