跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Continue to use E8 for MCUs supported by E8a

Last Updated:10/18/2017

Question:

I am currently using E8. Will E8 be able to debug new MCUs even after E8a is available?

Answer:

E8 will only support the MCUs listed on the E8 Products page.

The last MCU to be added to the E8 support list was Rev.2.11 Release 00, released in April 2008, and we have no plans to release any more E8-compatible MCUs. Please use the E8a emulator for any future system developments.

For details on the migration path from E8 to E8a, click here.

Suitable Products

E8
E8a