跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

"Circuit board is not operating as I am using emulator to debug. "

Latest Updated:10/16/2013

Question:

I’m using an emulator (e.g., E1, E20, and IECUBE) to debug.
Although the program is operating in CubeSuite+ (debug tool) after it was downloaded, the actual circuit board is not operating.
Furthermore, when the E1 or the E20 is used, the RESET lamp does not go out and the RUN lamp is not lighted.

Answer:

It is possible that the program is downloaded into a simulator. Check to see if the debug tool selected in the project tree is the emulator you’re using.

To select a debug tool, follow the procedure below.

[How to select a debug tool]
Select a debug tool in the project tree and right-click on it.
-> Select [Debug tool to use]
-> Select the tool you’re actually using.

Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]
IE850 (formerly IECUBE2)
IECUBE