跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Specifying Security ID_CC-RL

Last Updated:02/07/2018

Question:

I am using RL78 compiler CC-RL.
A security ID value is specified in the assembly source file, but the value is not reflected. How do I resolve this?

Answer:

If a security ID value is specified both in the assembly source file and by the -SECURITY_ID option of the linker, the specification of the option takes priority.
Thus, to specify the security ID in the assembly source file, delete the specification of the -SECURITY_ID option.


Suitable Products

e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family