跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

License purchased before the division into Standard and Professional editions

Last Updated:05/17/2017

Question:

How can I use a license purchased before the division into Standard and Professional editions?

Answer:

You can use it as the Professional edition.

Re-register the license as follows.

  1. Start up the license manager from the start menu of Windows. 
    *There are shortcuts for license manager under “Renesas Electronics CS+” for CS+, and under “Renesas Electronics Compiler” for compilers without an IDE.
  2. Deregister the registered license once, and re-register the license key which was previously registered.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family