跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Guidelines regarding the quantity of floating licenses to purchase?

Last Updated:05/17/2017

Question:

Do you have any guidelines regarding the quantity of floating licenses to purchase?

Answer:

We have no guidelines on that point. You need to consider the number of developers and the scale of the system you are developing when deciding on the number of licenses to purchase.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 这篇文章对您有帮助吗?