跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Evaluation edition of the Professional edition

Last Updated:05/17/2017

Question:

Do you have an evaluation edition of the Professional edition?

Answer:

Yes, we do. You can try the evaluation edition. The evaluation edition can be used as the Professional edition for 60 days from the first build after installing it.

In the evaluation edition, the features of the Professional edition will become no longer available and the linkage size will be restricted on and after the 61st day.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 这篇文章对您有帮助吗?