跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

E0210010 Message_CC-RL/CC-RX/CC-RH

Last Updated:12/06/2017

Question:

I got the following error. How do I resolve this?

“This operation has been cancelled because not currently allowed to disconnect from the debug tool. (E0210010)”
 

Answer:

[Explanation] This message appears when disconnection of the debugging tool was attempted even though this was not allowed.

[Action by user] Stop the debugger if it is operating.

See also “CS+ Integrated Development Environment User’s Manual: Message” for your reference.
 

Suitable Products
C Compiler Package for RL78 Family
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
RL78 Family
RH850 Family
RX Family
  • 这篇文章对您有帮助吗?