跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Confirming the value of the option byte using a program (CC-RL)

Last Updated:06/14/2017

Question:

I am using the RL78 compiler CC-RL. How can the value of option byte be read while a MCU is operating?

Answer:

The option byte area is the address that is not included in the mirror area of MCU (ROM).

Therefore, the far pointer should be used to access.

(For example) If you want to read the value of address 0C2h:

volatile unsigned char opdata;
opdata = (*(volatile __far unsigned char *)0x00c2);

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 这篇文章对您有帮助吗?