跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I add a license after purchasing a floating license?

Last Updated:05/17/2017

Question:

Can I add a license after purchasing a floating license?

Answer:

Yes. Purchase any product with or without a medium, then add to the number of licenses by registering the license key with the software for license management on the server PC.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family