跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Acquiring Annual License Key

Last Updated:11/29/2017

Question:

I have purchased an annual license. How do I acquire a license key to be registered in the tool?

Answer:

Log-in to MyRenesas and select the [Obtaining a Subscription License Key] menu.
Click the Add button to register the code for obtaining the license which accompanies the product, then the license key will be generated.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 这篇文章对您有帮助吗?