跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why do H8S/2xxx DTC has delayed some files including transfer and read?

Latest Updated:03/18/2009

Question:

On the H8S/2xxx DTC operation there is s one-cycle delay between the vector read and transfer information read. Why ?

Answer:

Address calculation.
Suitable Products
H8S Family