跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Which clock does the CPU operate with after reset release?

Latest Updated:02/27/2012

Question:

Which clock does the CPU operate with after reset release?

Answer:

After reset, the 125 kHz on-chip oscillator divided by 8 is used as the CPU clock.
Suitable Products
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57