跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Where to find the input/output data for Super Low Power Microcomputer?

Latest Updated:03/25/2009

Question:

Where can I find the input/output characteristics data for Super Low Power Microcomputer?

Answer:

Please refer to the input/output characteristics data available on the characteristic information page in this site. Please read the cautions before using the information.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power