跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

When does the operation count starts? Is it in timer 1, timer 2 or timer 3?

Latest Updated:01/17/2005

Question:

(Timer)   Prescaler, timer 1, timer 2 and timer 3 count start timing and count time when operation starts. [2005/01/17]

Answer:

 

Count starts from the first rising edge of the count source (2) after prescaler, timer 1, timer 2 and timer 3 operations start (1).
Subject to the operation start timing of the timers and count source, after count starts, the time to the first underflow (3) is (up to 1 count period) shorter than the time between subsequent underflows (4). (#105074)

Suitable Products
4571