跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What will happen if SKs executed after using stack pointer SP = 7?

Latest Updated:09/27/2004

Question:

(CPU)   The stack registers (SKs) are eight identical registers. If a stack use command is executed after using eight identical registers (stack pointer SP = 7), what will happen? [2004/09/27]

Answer:

The value of the SP will be set to 0, and the value in register SK0 will be overwritten. (#105048)
Suitable Products
4508
4509
4559
455A
4571