跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What should the SFR settings be for unused functions?

Latest Updated:09/29/2006

Question:

(Special Function Register(SFR))  What should the SFR settings be for unused functions ? [2006/09/29]

Answer:

Set to the same values as the initial values at reset. (#106376)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549