跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is 100% PWM output possible by setting the same value to CMP00 and CMP01?

Last Updated:12/26/2017

Question:

I want to execute the PWM output using the timers H0 and H1 in the 78K0/KC1.
Is 100% output possible by setting the same value to CMP00 and CMP01?

Answer:

No, it is not possible.
The value set to CMP01 must be smaller than the value set to CMP00; the same value cannot be set.
Suitable Products
78K0/Dx
78K0/Fx
78K0/Ix
78K0/Kx
78K0/Lx
UPD78F07xx
UPD7800xx
UPD7802xx
UPD7803xx
UPD7807xx
UPD7808xx
UPD7809xx
UPD780xx
UPD78F8025
78K0/VAN ASCP