跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the value of internal registers of power on reset?

Latest Updated:03/24/2009

Question:

After the power on reset, what is the value of internal registers at power-on reset?

Answer:

(1) On-chip I/O registers are set to the initial value (There are exceptions for some cases. For more information, please refer to the hardware manual.)

(2) CPU register: PC is loaded from vector table, I bit = 1 in CCR, others such as from R0 to R7 and CCR are undefined

Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power