跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the status of the ports during on-board flash programming?

Latest Updated:12/01/2011

Question:

During on-board flash programming, what is the status of the ports that are not related to programming?

Answer:

The ports that are not used during programming remain in their after-reset status, in other words, they are input ports.
Suitable Products