跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the stable oscillation time when using a ceramic oscillator?

Latest Updated:10/19/2004

Question:

(Clock)  What is the stable oscillation time when using a ceramic oscillator ? [2004/10/19]

Answer:

Since stable oscillation time differs depending on the oscillator and operating conditions, please consult with the manufacturer of your oscillator. Reference data can be found on our website by clicking "Reference Oscillation Circuit Constants" in the left side menu on the page of each Group. (#104922)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549
  • 这篇文章对您有帮助吗?