跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the pin state when switching a port to the SOUT pin after reset?

Latest Updated:11/12/2004

Question:

(Serial Interface)  What is the pin state when switching a port to the SOUT pin after reset? [2004/11/12]

Answer:

The pin is in high impedance state.
Bit 0 of the serial I/O register is output at the falling edge of the synchronous clock. Also, serial I/O register values are undefined after reset. (#105059)
Suitable Products
4508
4509