跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the maximum speed of the serial ports of H8/300L ?

Latest Updated:03/18/2009

Question:

What is the maximum speed of the serial ports on the H8/300L ?

Answer:

Most of the serial ports available on the H8/300L family can operate in either synchronous or asynchronous ( UART ) mode. In sync mode the maximum data rate is 2 Mbps with a 16 MHz crystal and in async mode the maximum data rate is 250 kbaud at 16 MHz.
Suitable Products
H8/300L Super Low Power
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power