跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the initial value of user program area in default setting?

Latest Updated:03/24/2009

Question:

What is the initial value of the user program area in the default factory setting?

Answer:

The data of the user program area in the default factory setting is FFh.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N