跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the difference between H8SX/1600 and H8SX/1500?

Latest Updated:05/07/2007

Question:

What is the difference between H8SX/1600 and H8SX/1500?

Answer:

H8SX/1600 Series provides a maximum operating frequency of 50 MHz*1 and external expansion function.
H8SX/1500 Series provides a maximum operating frequency of 48 MHz*2 and single chip*3 MCU.
*1:H8SX1650 and 1657F provide a maximum operating frequnecy of 35 MHz.
*2:H8SX1527F provides a maximum operating frequnecy of 40 MHz.
*3:Single chip MCU does not have external expansion function.
Suitable Products
H8SX/1663
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622