跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is Full-scale error?

Latest Updated:08/01/2005

Question:

What is Full-scale error?

Answer:

Full-scale error indicates the offset error (%FSR) between analog input when the maximum conversion value is reached and full-scale (FS) analog input (VREF) in an A/D converter. The full-scale error, zero-scale error, and non-linearity (linear) error constitute the overall error. This overall error does not include the quantization error that inevitably occurs during digital conversion.

Suitable Products
  • 这篇文章对您有帮助吗?