跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What could be the causes if hardware reset does not operate correctly?

Latest Updated:10/10/2006

Question:

The hardware reset does not operate correctly. What could be the causes?

Answer:

First, please verify that the program jumps to the address indicated by the reset vector.

  1. If the program does not jump to the appropriate address, verify that reset input is not against regulations.
  2. If the program malfunctions after jumping to the address, verify that the stack pointer and interrupt vector table are set correctly.

Also, the watchdog timer of the models other than R8C/10 and R8C/11 groups automatically operates, if the bit of FFFFh address of the flash memory is set to "0". Please check the value of FFFFh address.

Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC