跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What causes change in accuracy, precision of oscillator's frequency?

Latest Updated:08/05/2009

Question:

(Oscillation Circuit)
What causes variation in the accuracy and precision of the on-chip oscillator's frequency? [2009/08/05]

Answer:

General causes of variation are:

  • Manufacturing variation (chip variation)
  • Variation caused by supply voltage fluctuation
  • Variation caused by ambient temperature

For rated values, refer to "Electrical Characteristics" in each product's datasheet and user's manual.

(#107436)

Suitable Products
3823
38D2
38D5
7544
7546
7547
7548
7549