跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What are the definitions for dominant, recessive, SOF, and EOF?

Latest Updated:03/22/2017

Question:

What are the definitions for dominant, recessive, SOF, and EOF?

Answer:

Normally, dominant represents "low" and recessive represents "high".
Dominant is stronger than recessive on the bus. SOF, which is the abbreviation for Start-Of-Frame, indicates the start of a data frame or remote frame, and consists of one dominant bit. EOF stands for End-Of-Frame and consists of seven data bits. ACK is just one bit. Each data frame and remote frame is separated by an EOF flag consisting of seven recessive bits.

Suitable Products
R8C/22
R8C/23
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/1N