跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What's the setting of pull up when using P4_4 to P4_7 as a CS pin?

Latest Updated:02/27/2012

Question:

When using the P4_4 to P4_7 as a CS pin, is the setting of the pull-up invalid?

Answer:

When CS output is selected, the internal pull-up is invalid.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/30P