跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What's the recommended oscillator configuration for Tiny devices?

Latest Updated:03/18/2009

Question:

What is the recommended oscillator configuration for Tiny series devices ?

Answer:

The Renesas users manuals for each of the Tiny series devices has a example circuit for the oscillator, however you should discuss with your crystal or resonator supplier the best configuration of oscillator circuit for that specific crystal or resonator.For instance, Murata have a very useful website at http://www.murata.com/ ,where they have many circuit examples.
Suitable Products
H8/300H Tiny