跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What's the difference between 0.35μm boot mode and user program mode?

Latest Updated:01/18/2008

Question:

What's the difference between 0.35μm process version Flash memory boot mode and user program mode?

Answer:

In boot mode, the user transfers write control programs from host to MCU internal RAM via SCI or USB and, after a full erase of the Flash memory, enacts the write control programs. In user program mode, Flash memory write/erase is performed by the write/erase program(s) prepared by the user.
Suitable Products
H8S/2678, 2678R
H8S/2668
H8S/2649
H8S/2648, 2646
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2378, 2378R
H8S/2368
H8S/2398, 2357
H8S/2339
H8S/2329
H8S/2319
H8S/2282, 2280
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2215
H8S/2214
H8S/2218, 2212
H8S/2148, 2144
H8S/2140B
H8S/2138, 2134
H8S/2128, 2124
H8S/2111B
H8S/2110B