跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Should the data written in ID code area be deleted in QzROM version?

Latest Updated:02/26/2007

Question:

(ROM)  Regarding switching from Flash Memory version to QzROM version: Since the ID code check function is used in the Flash Memory version, ID and other data are written to the ID code store addresses and ROM code protect (addresses FFD4 to FFDBh). Should these data be deleted in the QzROM version ? [2007/02/26]

Answer:

It is not necessary to delete any addresses up to FFDAh. Set FFh to address FFDBh. (#106583)
Suitable Products
3803H
38D2
38D5